USA

Schneider Electric USA Website

Welcome to our website.

To view product availability in a specific country, select from the country list below. For Investor Relations, please visit our global site.

Choose another country or region

  • Default Alternative Text

    Packaging Automation Solutions

    Effective automation of packaging machines of all kinds and at every level of complexity

    + Lifecycle Services

#1 – Processing & Conveying

  • Roller Conveyor

    Roller conveyors are driven either by flat, cylindrical belts or by chains. They accommodate conveying line switches and sorters. Roller conveyors have a motor inside the rollers which propels loads across zones of conveyor sections.

    Default Alternative Text
  • Belt Conveyor

    Belt conveyor is a machine transporting material in a continuous way by friction drive. It is mainly composed by rack, conveyor belt, belt roll, tensioning device and gearing. It can form a material delivery process between the initial feeding point and the final discharging point.

    Default Alternative Text
  • Product Architecture

    Schneider Electric offers a complete line of products to meet your processing and conveying application needs, from machine energizing, emergency stop devices, servo motors, to controllers, HMI and signaling.
    Click the links below to learn more about our products:

    Default Alternative Text

    #2 – Feeding & Loading

      #3 – Vertical & Horizontal Form Fill & Seal

      • Vertical Form Fill & Seal

        Vertical/Horizontal Form Fill and Seal (VFFS/HFFS) machines are automated packaging systems used in packaging solid or liquid materials. VFFS/HFFS machines package product in a vertical or horizontal plane around a solid product using a film reel.
        The film tension is kept constant by means of a tension arm. The forward movement of the film drive motor during the bagging reduces the film reserve and lifts the tension arm. When the arm reaches its top position, a portion of the film on the reel is unwounded to fill again the film reserve until the tension arm reaches its initial (bottom) position. The film is folded to envelop the product and then sealed alongside.
        A conveyor moves the products to the center of the film. The transverse sealing wheels close the back part of the bag; the cutter cuts off the full bag that then is evacuated on another conveyor. The cut in the middle of the sealing also allows to close the front part of the next bag.

        Default Alternative Text
      • Horizontal Form Fill & Seal

        Vertical/Horizontal Form Fill and Seal (VFFS/HFFS) machines are automated packaging systems used in packaging solid or liquid materials. VFFS/HFFS machines package product in a vertical or horizontal plane around a solid product using a film reel.
        The film tension is kept constant by means of a tension arm. The forward movement of the film drive motor during the bagging reduces the film reserve and lifts the tension arm. When the arm reaches its top position, a portion of the film on the reel is unwounded to fill again the film reserve until the tension arm reaches its initial (bottom) position. The film is folded to envelop the product and then sealed alongside.
        A conveyor moves the products to the center of the film. The transverse sealing wheels close the back part of the bag; the cutter cuts off the full bag that then is evacuated on another conveyor. The cut in the middle of the sealing also allows to close the front part of the next bag.

        Default Alternative Text
      • Product Architecture

        Click to learn more about our products:


        Machine Energizing - TeSys D Contactors, TeSys GS, Vario Switches, FA Molded Case Circuit Breakers, PowerPact B-Frame Molded Case Circuit Breakers
        Emergency Stop – Preventa XPS
        Film Unwind Servo Motor – Lexium 28
        Film Drive Servo Motor / Sealing Jaw Servo Motor – Lexium 32
        Controller – PLC
        HMI – Magelis
        Control and Signaling – Harmony C&S Products

        Default Alternative Text

        #4 – Filling & Capping

          #5 – Price Labelling & Shrink Sleeving

            #6 – Flow Pack

            • Flow Pack

              Check back for more solution information

            #7 – Wrap Around Boxing

            • Wrap Around Boxing

              Machine forms a box around a batch of products and then to close it. Transfer of the batch results in the box wrapping itself around the latter, either by vertical transfer (described here) or lateral transfer. This boxing system is suitable for packaging in general and has the advantage of minimizing the play of products in their box.

              Default Alternative Text
            • Product Architecture

              Click to learn more about our products:


              Machine Energizing - TeSys D Contactors, TeSys GS, Vario Switches
              Machine Drive –
              Altivar 320, Altivar 340
              Movement Supply and Safety Cut-Off – TeSys D Contactors
              Controller – PLC
              HMI – Magelis
              Control and Signaling – Harmony C&S Products

              Default Alternative Text

              #8 – Grouping / Ungrouping Machine

                #9 – Shrink Wrapping

                  #10 – Parceling

                    #11 – Pallet Dispenser

                      #12 – Palletizing

                        #13 – Automatic Storage & Retrieval System (ASRS)

                        • ASRS

                          The transtorage system consists of a self-propelled column moving along a central aisle (traverse). It supports a vertically sliding platform (lifting). The extraction movement (direction) brings a bin from the stock to the platform and vice versa. Some storage systems can change aisles by curved paths and switches.

                          Default Alternative Text
                        • Product Architecture

                          Click to learn more about our products:


                          Machine Energizing - TeSys D Contactors, TeSys GS, Vario Switches
                          Movement Supply and Safety Cut-Off – TM5 Safety
                          Film Drive Servo Motor / Sealing Jaw Servo Motor – Lexium 32
                          HMI – Magelis
                          Control and Signaling – Harmony C&S Products

                          Default Alternative Text

                          #14 – Stretch Wrapping

                          • Rotary Arm

                            Stretch machines wrap palletized loads in stretchable plastic film (polyethylene) by rotating a reel-holder around the pallet (rotary arm) or rotating a pallet itself.
                            The top cover is applied to the material; the stabilizer plate descends until it is in contact with the load. The fastening of the film is automatically carried out by an arm. The rotary arm starts to apply the plastic film around the pallet.

                            Default Alternative Text
                          • Rotary Pallet

                            Stretch machines wrap palletized loads in stretchable plastic film (polyethylene) by rotating a reel-holder around the pallet (rotary arm) or rotating a pallet itself.
                            Stretch wrap with a rotary pallet starts with fastening the film to the pallet. When machine cycle starts, the rotation of the table wraps the film around the table. The reel-holder carriage moves regularly upwards/downwards so that the pallet is spirally wrapped.

                            Default Alternative Text
                          • Product Architecture

                            Click to learn more about our products:


                            Machine Energizing - TeSys D Contactors, TeSys GS, Vario Switches, FA Molded Case Circuit Breakers, PowerPact B-Frame Molded Case Circuit Breakers
                            Movement Supply and Safety Cut-Off – Preventa XPS
                            Arm Rotation – TeSys D Contactors, TeSys U Combination Motor Starter
                            Lifting of reel-holder carriage – Altivar 320, Altivar 340
                            Lifting/lowering of film reel to make up top cover – Altivar 320, Altivar 340
                            Drive of roller conveyor – Altivar 320, Altivar 340
                            Pre-stretching of film – Altivar 320, Altivar 340, Lexium 28
                            Controller – PLC
                            HMI – Magelis

                            Default Alternative Text