Technical FAQs

Ask a Question

Filter results

Clear
What are the replacement modules for a FI8IMA12 or FI8IMA12C and FI8IMA16 or FI8IMA16C?
Product Line: Surge Protective Devices (SPDs) Environment: Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can...
What are possible causes for over braking faults, OBF, on the ATV61 or ATV71 drives?
Issue: Possible causes for over braking faults, OBF, on the ATV61 or ATV71 drives . Product Line: ATV61   ATV71 Environment: All Cause: DC Bus voltage...
What terminals on an Altivar drive do I connect a braking resistor to?
Issue: What terminals on an Altivar drive do I connect a braking resistor to? Product Line: ATV312, ATV32, ATV61, ATV71, ATV630, ATV930, ATV320 Environment:...
ATV320: Where is the brake resistor installed?
Issue: On the ATV320 drives, to what terminals are the Braking resistor connected? Product line: ATV320, Altivar 320 Environment: all Cause: Adding...
Is there a problem using Altivar 61 or Altivar 71 drives delta power system?
Issue: IWants to use Altivar 61 or Altivar 71 drives on delta power system. Product Line: Altivar ATV61 and ATV71 Environment: All Cause: Needs to...
How are wires terminated under binder screws on an 8910 ?
Issue: Terminations Product Line: Contactors Environment: 8910 DP Cause: Wiring Resolution: Use spade or eye type wire connectors or lugs
Are lugs included with ATS22 Soft Starts?
Issue: Are lugs included with ATS22 Soft Starts? Product Line: ATS22 Environment: All Cause: N/A Resolution: Smaller units (ATS22D17 thru ATS22D88)...
How is damper control configured on the ATV212 series drive?
Issue: How is damper control configured on the ATV212 series drive? Product Line: Altivar 212 series drives.   Environment: All models and serial...
Does the ATS48 unit provide separate power terminals to connect cables that feed the line side of the shorting contactor?
Issue:  Does the ATS48 unit provide separate power terminals to connect cables that feed the line side of the shorting contactor? Product Line:  ATS48...
Will the measurement of the 24V on an Altivar drive be different if referenced from earth ground as opposed to the COM terminal of the drive?
Issue: Reference point for the 24V power supply. Product Line: Altivar VFD Environment: All models and serial numbers with the exception of the ATV11. ...
Results 1 - 10 of 100