Technical FAQs

Ask a Question

Filter results

Clear
Does the Schneider Electric repair depot repair ATS22 soft starts?
Issue: Does the Schneider Electric repair depot repair ATS22 soft starts? Product Line: Altistart 22 Environment: All Cause: ATS22 needs repair Resolution:...
Where do I check for a last fault code on an ATV31 and ATV312 drives?
Issue:  No fault code displayed, after drive reset. Product Line: ATV31 and ATV312 Environment:  All Cause:   Would like to know the last drive fault...
What is the phone number for MTE?
Issue: What is the phone number for MTE?   Product Line: N/A   Environment: All   Cause: Contact information for MTE Corp   Resolution: Toll Free:...
What would cause an ATV61 (or ATV71) to trip on Ground short circuit (SCF3) fault?
Issue: What is an SCF3 fault on the ATV61 and ATV71 drives? Product Line: Altar ATV61 ATV71 Environment: All Cause: Ground Short Circuit fault Resolution:...
What's the difference between ATS22..S6U and ATS22...S6 Softstart models?
Issue: What's the difference between an ATS22..S6U and  ATS22..S6 soft start models? Product Line: Altistart 22 ATS22 Environment: All models, All...
Why is the ATV312 tripping on SCF or short circuit fault on power up?
Issue: Why is the ATV312 tripping on SCF or short circuit fault on power up?  Product line: Altivar 312, ATV312, ATV31 Environment: All models, all...
Firmware version 1.60 for FFTK
Issue:  Where can I find FFTK firmware version 1.60 to download? Product Line: Circuit breakers Resolution: You may download the firmware from this...
Can the I-Line shroud or jaws on an I-Line circuit breaker be replaced?
Product Line: Legacy and Powerpact Circuit Breakers Resolution: No, this is not possible.  
I replaced the motor connected to my Lexium 05 drive and now see "not" on the display
When replacing a motor that is connected to Lexium 05 you will see "not" on the display if the replacement motor is not the same motor type as the...
Who provides support for class 2830 meters used in panelboards, switchboards, and motor control centers?
Square D / Schneider sold this product line in 1988 to Modutec / Jewell Electric Instruments. Users of these products can contact Modutec / Jewell...
Results 1 - 10 of 100