Technical FAQs

Ask a Question

Filter results

Clear
How many OF aux. switches may be added to the Masterpact NW breaker?
Product Line: Circuit Breakers Environment: Applies to Masterpact NW circuit breakers. Resolution: Four are standard: 4a4b form C. Two additional...
Does Square D offer a NQ Panel board with a QO/QOB 2 Pole GFI Circuit Breaker Series rated above 10,000 AIC?
Issue: Does Square D offer a NQ Panel board with a QO/QOB 2 Pole GFI Circuit Breaker Series rated above 10,000 AIC? Product Line: Panelboards. Environment:...
How to set low speed on the ATV21/212?
Issue: How to set low speed on the ATV21/212?    Product line:   ATV21, ATV212 Environment:   All models, all serial numbers Cause: Program the lowest...
What are the replacement modules for a FI8IMA12 or FI8IMA12C and FI8IMA16 or FI8IMA16C?
Product Line: Surge Protective Devices (SPDs) Environment: Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can...
Is an Analog Output standard on the ATS48 unit?
Issue: Analog Output standard on the ATS48 unit? Product Line: Altistart 48 Environment: All Cause: Need details on analog output Resolution: Yes....
Does Square D offer a meter socket 'jumper' cover that allows power (current) to pass through a meter socket without a Watt-hour meter installed?
Issue: Meter Socket 'Jumper' Cover for the Metering Equipments Product Line:  Metering Equipment Environment: EZM Metering and MP Meter-Pak Metering...
Is there a test kit for Micrologic trip units for the PowerPact H, J and L frame circuit breakers?
Product Line: PowerPact H, J and L frame breakers with Micrologic Trip Units Environment: PowerPact H and J frame breakers with Micrologic trip units...
​Is Smoke Purge Option available on ATV660 Enclosed Drives?
Issue: ​Is Smoke Purge Option available on ATV660 Enclosed Drives? Product Line: ATV660, Altivar 660 Environment: All Cause: Smoke Purge option is...
ATV660: Are Seismic options available?
Issue: Customer is building ATV660 but the Selector tool does not allow the option for form H10 for Seismic qualifications. Product line: ATV660,...
Are any of the Square D Heavy Duty Safety Switches available without a dual cover interlock?
Issue: Product design features Product Line: Heavy Duty Safety Switches Environment: Mounting Cause: Application Resolution: NO, ALL the Heavy Duty...
Results 1 - 10 of 100