Technical FAQs

Ask a Question

How can a Powerpact P or R frame breaker with a 3.0 trip unit be modified to have ground-fault indication.
Product Line: Circuit Breakers Environment: Electrical Distribution Equipment Resolution: Replace the trip unit with a 5.0P trip unit (S163A) and...
Is the trip unit on a Powerpact M, P and R with ET1.0I trip unit replaceable?
Product Line: Circuit Breakers PowerPact M, P, and R Envrionment: Electrical Distribution Equipment. Resolutions: The basic electronic trip unit ET1.0...
When did the ATS46 soft start become obsolete?
Issue: Customer would like to know when the ATS46 became obsolete. Product line: ATS46, Altistart 46 Environment: All models. Cause: Determine age...
When did the ATS23 soft start become obsolete?
Issue:    When did the ATS23 soft start become obsolete?   Product Line:   ATS23   Environment:  All   Cause:   N/A   Resolution:    ATS23 became...
Does Schneider Electric offer replacement jog dials for the ATV12 drive?
Issue: Replacement jog dial for the ATV12 drive Product Line: Altivar 12 drives Environment: All models and serial numbers Cause: None Resolution:...
How can the price for an enclosed drive or enclosed Soft Start package be obtained?
Issue: Customer is trying to find pricing for an enclosed drive or enclosed Soft Start. Product Line: ATV660 ATV960 Altivar Process E-Flex M-Flex...
Did Square D offer Arc Fault branch breakers for the Trilliant plastic load centers?
Issue: Arc fault breakers for Trilliant load centers. Product Line: Load Centers Environment: Trilliant Load Centers Resolution: No, Square D did...
What drive replaces the ATV58 or ATV66 Product Line?
Issue:  Needs a drrive replacement for the ATV58 or ATV66 Product Lines. Product Line:  ATV58, Altivar 58, ATV66, ATV56, Altivar 66 Environment All...
Does a fire pump circuit breaker need to have a red handle?
Issue: How to identify a fire pump circuit breaker? Product Line: Molded Case and Miniature Circuit Breakers Environment: Requirements for Fire Alarm...
Can I Line Busplug switches be installed on Busway running vertically?
Issue: Installing a PQ4610G plug-in unit on a vertically mounted Busway. Product Line: I-Line NEMA Busway Environment: Busplug flexibility in mounting...
Results 1 - 10 of 100