Technical FAQs

Ask a Question

Filter results

Clear
Are the new Powerpact I Line breakers securely mounted when the mounting foot screw falls into the slot next to the hole that was used with the Legacy breakers, FA,KA?
Issue: Are the mounting foot screws for Powerpact I-Line breakers (H, J and L-frame) supposed to thread into the same holes in the back of the panelboard...
On Powerpact M, P and R frame circuit breakers, is it ok if there is some movement on the bottom terminals (OFF end) of the breaker?
Issue: Are the bottom terminals on the M, P and R breaker supposed to be loose? Product Line: Circuit Breakers Environment: Powerpact M, P and R Resolution:...
Can the Powerpact J frame breaker be used in the N600SFBKC?
Issue: Can Powerpact J breakers be used in the N600SFBKC? Product Line: NF subfeed breaker kits Environment: N600SFBKC and NF600SFBJ Cause: Product...
What is the correct Depth dimension for NEMA 3R/12 NQ Panelboard enclosures? Is it 6.5'' deep per Digest 176 , Page 9-7 , or 6.25" per the Engineering drawing PBA711 ?
Issue: Engineering drawing PBA711 shows Depth of MH**WP box as 6.25",  and the 176 Digest lists the MH**WP panel box as 6.5"D , which is correct?...
Video: How do you get cross reference assistance for items that are not in the cross reference tool?
Issue: How do you get cross reference assistance for items that are not in the cross reference tool? Product Line: All products Environment: Cross...
How do I back-fed a branch breaker into a HOM612L100F, HOM612L100S, or HOM612L100RB?
Issue: Where does the back-fed main breaker install into in a HOM612L100F, HOM612L100S or HOM612L100RB series 001 (or 1) load center? What is the...
Need part number for cover mounting screws for Powerpact P frame breaker ?
Product Line: Circuit Breakers Environment: Applies to Powerpact P circuit breakers. Resolution: Part number 04444957AA is for one screw. Contact...
Can the DC bus on the ATV630 process drives be shared?
Issue: Can the DC bus on the ATV630 process drives be shared? Product Line: ATV630 Environment: All models and serial numbers Cause: None Resolution:...
What does the 'U' suffix mean at the end of the ATS48 Soft Starters' part numbers?
Issue: What does the 'U' suffix mean at the end of the ATS48 Soft Starters' part numbers?  Product Line: Altistart 48 Environment: All models. Cause:...
Does the LAD9R1 or LAD9R1V mechanical interlock fit the Pre TeSys LP1D and LC1D 9-32A type contactors?
Issue: Pre Tesys LP1D and LC1D 9A - 32A accessory compatability Product Line: IEC contactors and starters Environment: TeSys and Pre TeSys LC1D and...
Results 1 - 10 of 100