{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

What would cause a EPF2 fault using Profinet's telegram 1 and I/O profile...

Issue: EPF2 fault causes using Profinet and I/O profile on the ATV630 and ATV930 drives. Product Line: ATV630, ATV930 Environment: All Cause: IO Profile and Telegram 1 are not compatible. Resolution:...

What is the ``PBT`` material used in the face of the XS1N08PA349 sensor?

Issue: What does PBT stand for? Product Line : OsiSense XS Environment : Inductive proximity sensor Resolution : It is a polyamid plastic, PolyButylene Teraphalate Polyester.

What are the part numbers for the remote keypad and mounting accessories...

Issue : What are the part numbers for the remote keypad and mounting accessories for Altivar Process Drives? Product Line : Altivar Process Drives Environment : Keypad Cause : Remote mounting...

What is the Part Number to unlock the WebViewer feature for Harmony...

Issue In order to unlock the WebViewer feature in the Harmony HMIST6, HMISTM6, or iPC what is part number of the License? How is it unlocked on an iPC? Product Line Harmony HMIST6 (HMIST6200,...

Voltage Inputs Burden Rating for ION and Powerlogic Meters

Issue Burden rating for the voltage input terminals. Product Line ION6200, ION75xx, ION76xx, ION86xx, PM5xxx, PM8xxx, PM8xx Resolution The voltage input terminals for the Powerlogic and ION meters...

What is the part number of the replacement contacts for LC1FG43?

Issue: Are the contacts on an LC1FG43 replaceable? Product Line: Tesys F line Contactors and Accessories Environment: Products sold in the US Resolution: This contactor is already obsolete, the...

What is the part number for the bus bar screws to connect QOB breakers to...

Issue: Replacement for the bus mounting screws to connect QOB breakers to an NQ panel Product Line : QOB breakers Environment: Applies to QOB breakers only. Cause: The bus bar screw is missing or...

What is the warranty period for units installed in Puerto Rico?

Issue: Minimum warranty period for solar products in Puerto Rico Product Line: XW/XW+, Conext SW Series Inverter/charger, XWMPPT etc. Environment: Applications where solar grid tie and battery based...

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our General Knowledge FAQsGeneral Knowledge

How to have access to M218 controllers in Machine Expert

The M218 controllers are not sold or supported in the US, they are only sold and supported in Asia. So to have access to them you will need to use the Local Offer code that you enter to unlock it...

What is the difference between PNP and NPN when describing 3 wire...

Most industrial proximity sensors (inductive, capacitive, ultrasonic and photo electric) are solid state. The term solid state refers to the type of components used within the sensor. Solid state...

What do the terms AC1 and AC3 mean?

Issue: What are the utilization categories AC-1 and AC-3? Product Line: Schneider Electric Products Environment: Inductive and Resistive Loads Resolution: AC-1 - This category applies to all AC loads...

How do I become a supplier for Schneider Electric?

Issue: How to become a supplier for Schneider Electric Product Line: Source Materials Environment: Products sold and used in the United States Resolution: For information and help on becoming a...

What is Modbus and How does it work?

What is Modbus? Modbus is a serial communication protocol developed by Modicon published by Modicon® in 1979 for use with its programmable logic controllers (PLCs). In simple terms, it is a method...

What does the term "NEMA Type 1A" refer to?

NEMA Standards Publication 250-1997, "Enclosures for Electrical Equipment (1000 Volts Maximum)" no longer lists this enclosure type. This enclosure type is commonly accepted to be referring...

Where can I apply for a job with Schneider Electric?

Issue: How can I apply for a job? Product Line: Peoplelink Environment: Job opportunity Cause: Looking for location to apply for employment with Schneider Electric. Resolution: For career...

Insulation Resistance Testing and Humidity

Issue: How does humidity affect insulation resistance testing results? Product Line: Circuit Breakers Environment: Molded case and insulated case breakers Resolution: High humidity can drastically...