Technical FAQs

Ask a Question

What are LED status indications mean on the HMI screen of the Altivar 630 and 930 process drives?
Issue: Where can I get a documentation that explains the LED status indications on the HMI screen of the Altivar 630 and 930 process drives? Product...
Is it possible to compare or convert configurations from ATV61/71 to ATV6xx in SoMove?
Issue:   Can you compare or convert configurations from ATV61/71 to ATV6xx in SoMove? Product Line: Altivar 61, Altivar 71 , Altivar 630, Altivar...
Are Masterpact NW breakers primary injection tested in the factory.
Issue: Are the NW breaker primary injection tested at the factory before being sent out? Product Line: Masterpact NW Circuit Breakers Resolution:...
How do you program an auto/manual or com via digital input on the ATV630 and ATV930 Process drives?
Issue: Setup Hand off auto on the ATV630/ATV930 Process drives. Product Line: Altivar ATV630 ATV930 Process drive Environment: All Cause: Wants to...
Does Square D offer a meter socket 'jumper' cover that allows power (current) to pass through a meter socket without a Watt-hour meter installed?
Issue: Meter Socket 'Jumper' Cover for the Metering Equipments Product Line:  Metering Equipment Environment: EZM Metering and MP Meter-Pak Metering...
​Is Smoke Purge Option available on ATV660 Enclosed Drives?
Issue: ​Is Smoke Purge Option available on ATV660 Enclosed Drives? Product Line: ATV660, Altivar 660 Environment: All Cause: Smoke Purge option is...
What are the repair parts for a QO142L225PG, Series S06 Load Center?
Issue: Plug-On Neutral design repair parts Product Line: QO load centers Environment: Repair parts Cause: Maintenance Resolution: Only the parts listed...
DELETE: Is the door for an MH-WP NEMA 3R enclosure replaceable?
Issue: Lost or damaged door on NEMA 3R Weatherproof panelboard enclosure Product Line: Weatherproof Nema 3R/12 panelboard enclosures sold and supported...
What is the difference between the EX and newer EXN series Transformers?
Issue: For the EX and EXN transformers: What are the differences? Product Line: Low Voltage Transformers Environment: EX and EXN Resolution: The main...
What is the part number for a 1600A or above disconnect switch in a NEMA 3R enclosure?
Issue: How do you select a partnumber for a 1600A or above disconnect switch in a NEMA 3R enclosure? Product Line: Switchboard Environment: QED 2,...
Results 1 - 10 of 100