Technical FAQs

Ask a Question

Filter results

Clear
Can Powerpact H, J, and L frame breakers be applied at 400 Hz?
Issue:   H J L breakers at 400 Hz Product Line: Circuit Breakers Environment: Powerpact H, J, L Resolution: Yes, but with derating for both current...
Is it possible to use the Micrologic trip unit on a Powerpact or Masterpact circuit breaker to provide phase loss, phase reversal, or phase imbalance protection?
Issue: Is it possible to use the Micrologic trip unit on a Powerpact or Masterpact circuit breaker to provide phase loss, phase reversal, or phase...
What are LED status indications mean on the HMI screen of the Altivar 630 and 930 process drives?
Issue: Where can I get a documentation that explains the LED status indications on the HMI screen of the Altivar 630 and 930 process drives? Product...
Is it possible to compare or convert configurations from ATV61/71 to ATV6xx in SoMove?
Issue:   Can you compare or convert configurations from ATV61/71 to ATV6xx in SoMove? Product Line: Altivar 61, Altivar 71 , Altivar 630, Altivar...
How do you program an auto/manual or com via digital input on the ATV630 and ATV930 Process drives?
Issue: Setup Hand off auto on the ATV630/ATV930 Process drives. Product Line: Altivar ATV630 ATV930 Process drive Environment: All Cause: Wants to...
Can you replace or change out the trip units on the 500 Vdc breakers?
Issue: Can you replace or change out the trip units on the 500 Vdc breakers?   Product Line: Powerpact Circuit Breakers   Environment: 500 Vdc Circuit...
ATV660: Are Seismic options available?
Issue: Customer is building ATV660 but the Selector tool does not allow the option for form H10 for Seismic qualifications. Product line: ATV660,...
What are possible causes for over braking faults, OBF, on the ATV61 or ATV71 drives?
Issue: Possible causes for over braking faults, OBF, on the ATV61 or ATV71 drives . Product Line: ATV61   ATV71 Environment: All Cause: DC Bus voltage...
DELETE: Are PK**GTA ground bars UL508A listed?
Issue: Are PK**GTA  ground bars UL508A listed Product Line: Ground bars Environment: UL Classification  Cause: If ground bar kits are UL508A listed...
Are there any restrictions with mounting a QOB3125VH into an NQ interior?
Issue: Restrictions with mounting a QOB3125VH into an NQ interior Product Line: Panelboards Environment: NQ Panelboards Resolution: QOB3125VH takes...
Results 1 - 10 of 100