{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

What does the "R" (or "R-Handles" pointing to dash lines) printed on...

Issue: Installation of Replacement Tandem Breakers in non-Class CTL load centers Product Line: Load Centers Resolution: That marking is an indication of spaces in which tandem breakers (Replacement...

What causes an OPF1 fault on the AT12 drives?

Issue: Getting OPF1 fault on the AT12 drive. Product Line: ATV12 Environment: OPF1 faults Cause: 1 phase loss between the drive and motor. Resolution: This fault is triggered when the drive detects...

How to setup an ATV320 drive for Modbus control?

Issue: Programming ATV320 drives for Modbus control. Product Line: Altivar 320 Environment: All Cause: N/A Resolution: CONF, FULL, CON- ND1- menu tree. Parameter Add sets the Modbus address Parameter...

What is the difference between an XS1M18PA370 and an XS1M18PB370 ?

Issue: XS1M18PA370 and an XS1M18PB370 difference Product Line : Sensors Environment : North American Products Resolution : The first is a sensor with a N.O. (normally open ) output ( `` A `` means...

Window Server 2012 R2 No RDS license when you connect to a Windows Server...

Issue When attempting to remote into a Windows Server 2012 R2 server there is an error “Remote session was disconnected because there are no Remote Desktop client access licenses available for this...

What is the ``PBT`` material used in the face of the XS1N08PA349 sensor?

Issue: What does PBT stand for? Product Line : OsiSense XS Environment : Inductive proximity sensor Resolution : It is a polyamid plastic, PolyButylene Teraphalate Polyester.

What are the part numbers for the remote keypad and mounting accessories...

Issue : What are the part numbers for the remote keypad and mounting accessories for Altivar Process Drives? Product Line : Altivar Process Drives Environment : Keypad Cause : Remote mounting...

What is the Part Number to unlock the WebViewer feature for Harmony...

Issue In order to unlock the WebViewer feature in the Harmony HMIST6, HMISTM6, or iPC what is part number of the License? How is it unlocked on an iPC? Product Line Harmony HMIST6 (HMIST6200,...

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our General Knowledge FAQsGeneral Knowledge

How to have access to M218 controllers in Machine Expert

The M218 controllers are not sold or supported in the US, they are only sold and supported in Asia. So to have access to them you will need to use the Local Offer code that you enter to unlock it...

What is the difference between PNP and NPN when describing 3 wire...

Most industrial proximity sensors (inductive, capacitive, ultrasonic and photo electric) are solid state. The term solid state refers to the type of components used within the sensor. Solid state...

What do the terms AC1 and AC3 mean?

Issue: What are the utilization categories AC-1 and AC-3? Product Line: Schneider Electric Products Environment: Inductive and Resistive Loads Resolution: AC-1 - This category applies to all AC loads...

How do I become a supplier for Schneider Electric?

Issue: How to become a supplier for Schneider Electric Product Line: Source Materials Environment: Products sold and used in the United States Resolution: For information and help on becoming a...

What is Modbus and How does it work?

What is Modbus? Modbus is a serial communication protocol developed by Modicon published by Modicon® in 1979 for use with its programmable logic controllers (PLCs). In simple terms, it is a method...

What does the term "NEMA Type 1A" refer to?

NEMA Standards Publication 250-1997, "Enclosures for Electrical Equipment (1000 Volts Maximum)" no longer lists this enclosure type. This enclosure type is commonly accepted to be referring...

Where can I apply for a job with Schneider Electric?

Issue: How can I apply for a job? Product Line: Peoplelink Environment: Job opportunity Cause: Looking for location to apply for employment with Schneider Electric. Resolution: For career...

Insulation Resistance Testing and Humidity

Issue: How does humidity affect insulation resistance testing results? Product Line: Circuit Breakers Environment: Molded case and insulated case breakers Resolution: High humidity can drastically...