Browse FAQs

What linkage kit is used with a VB-9213-0-5-14 4" valve and MP-9750 Actuator ?

Published date: 08 October 2019

Issue:
Is there a linakge kit for the 2 1/2" -4" VB-9213-0-5-xx 2 Way valves?

Product:
Valves and Actuators 

Environment:
Maintenance

Cause:
Replacement

Resolution:
The linkage kit for the 2 1/2" -  4" , 2W mixing valve is no longer available, if possible, the old the linkage kit needs to be reused The new VB-9213 valve can be used with a M1500A, of MS41-6343 Actuators, but a new Controller would need to be adapted, since control signals are different between the MP-9750 and new actuators. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.