Browse FAQs

Is the DTU365 rated Service Entrance in Canada?

Published date: 08 October 2019

Issue:
Is the 400A DTU365 Service Entrance approved in Canada?

Product line:
Safety Switch

Environment:
Double Throw

Resolution:
Per the wiring diagram for the DTU365 states "Suitable for use as service equipment(USA ONLY)". So it is not service entrance rated for Canada. Also, keep in mind ALL the 600amp and 400amp Double throw switches are brand labeled from Cutler Hammer. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.