Browse FAQs

How Do I configure Pagefile Settings?

Published date: 06 October 2019

Product Line
PME 7.x, PME 8.x, PME 9.0, Windows Server 2008, 2012, 2016

Environment
Windows Server Performance

Cause
Pagefile filling up

Resolution
You can configure the page file by using System Properties:

  1. Run sysdm.cpl
  2. Go to Advanced
  3. Select Settings under Performance
  4. Go to Advanced (again)
  5. Select Change under Virtual Memory

Let's explore the different options:

 

  • System managed – This is the default option and recommended by Microsoft
  • Custom Size – Allows you to manually configure the size of the paging file
  • No paging file – Configure the system for not having a page file

When using System Managed, Windows determines the size of the page file based on the amount of physical memory


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.