Browse FAQs

What is part number ZBRA2?

Published date: 25 September 2019

Issue:
ZBRA2 function

Product line:
ZB5R XB5R Harmony Wireless

Environment:
Wireless pushbuttons

Cause:
Part shows a picture in the catalog but there is no description

Resolution:
ZBRA2 is an antennae to extend the range of the ZBRN1 and ZBRN2 modules.
A section from the ZBRN instruction manual, EIO0000001177.04, is attached to show the details.

Was this helpful?

What can we do to improve the information ?