Browse FAQs

Why are my Sub Scene POI's showing up on my Main Scene in EcoStruxure Augmented Operator Advisor?

Published date: 18 September 2019

Issue:
All points of interest defined in EcoStruxure Augmented Operator Advisor builder appear on the Main Scene when majority of the them were defined for a Sub Scene.

Product Line:
EcoStruxure Augmented Operator Advisor, EcoStruxure Augmented Operator Advisor Builder

Resolution:
When the images for the Main Scene and Sub Scene are very similar, it is possible that the app cannot distinguish between the two images and show all the POI's defined. The recommended way to design you app is to ensure the Sub Scene is an image that does not resemble the Main Scene. For example, you should zoom in on the section of interest for the machine for the Sub Scene rather than display the whole machine.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.