Browse FAQs

Does the TM221CE24T support thermocouple type K inputs

Published date: 18 September 2019

Issue:
Does the M221 support thermocouple  inputs.

Product Line:
M221

Resolution:
You can add the TMC2TI2 cartridge to the TM221C series. It will support 2 thermocouple or RTD inputs.
You can also use the following TM3 temperature input cards on all M221 PLC's.  TM3TI4D, TM3TI4, TM3TI8T and TM3TIM3
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.