Browse FAQs

Type of X80 Rack needed for BMEPXM0100 module

Published date: 11 September 2019

Title
Ethernet X80 Rack needed for BMEPXM0100 module
 
Issue
BMEPXM0100 module requires an Ethernet capable rack
 
Product Line
M580
 
Environment
Control Expert 14
 
Resolution
The PMEPXM0100 module requires an Ethernet capable backplane.
The Ethernet bus interface at the back of the PXM module connects to the Ethernet backplane connector when you mount the module in the rack.
There is no XBUS bus interface on the back of the PMEPXM0100 module. The module only uses the Ethernet bus interface on the rack.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.