Browse FAQs

Can I still use the manual charging handle on a breaker with a spring charging motor equipped?

Published date: 09 September 2019

Issue:
Manually charging breaker with spring charging motor equipped

Product Line:
Masterpact NW, Powerpact P, R

Cause:
Concern for damage to the mechanism

Resolution:
The manual spring charging mechanism can still be used when the spring charging motor is installed.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.