Browse FAQs

When using a VW3A3316 Ethernet IP option card in an ATV71, what do the status LED's indicate?

Published date: 03 September 2019

Issue:
What do the signaling LED's indicate when using a VW3A3316 Ethernet IP card?

Product Line:
Altivar 71, VW3A3316

Environment:
All

Cause:
Documentation of status LED indications

Resolution:
Please refer to the attached file, which is page 23 of the ATV61/71 Ethernet IP VW3A3316 User Manual.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.