Browse FAQs

Can the LTM9CU30 cable be used to connect the LTME and LTMR devices?

Published date: 21 August 2019

Issue:
Can the LTM9CU30 cable be used to connect the LTME and LTMR devices?

Product Line:
LTMR, LTME

Environment:
All

Cause:
N/A

Resolution:
No, the LTM9CU30 is not compatible to work between LTME and LTMR devices.  It only has 4 pins not 6 or 8.  This is cable is only compatible to be used between the keypad (if you have one) and expansion module or LTMR device, not between expansion and the LTMR device.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.