Technical FAQs

Ask a Question

Can the Ethernet version of the LTMR Tesys T product support Ethernet IP and Modbus TCP at the same time?

Issue:
Can the Ethernet version of the LTMR Tesys product support both Modbus TCP and Ethernet IP simultaneously?

Product Line:
LTMR Tesys T

Environment:
Ethernet IP / Modbus TCP version

Cause:
Clarification of product capabilities.

Resolution:
No.  The Ethernet version of the Tesys T will support either Modbus TCP or Ethernet IP.  This selection must be made when the Tesys is first being configured.  It will not support both Ethernet IP and Modbus TCP at the same time.
Was this helpful?
What can we do to improve the information ?