Technical FAQs

Ask a Question

Replacement for LXM15 drives

Issue:
Replacement for LXM15 drives

Product Line:
LXM15

Resolution:
Lexium 15 drives are now replaced by Lexium 32 drives. 
In order to make the proper selection, we need to know: 
- What is the model number of the servo motor currently in use and what is its date of manufacture? (see motor nameplate) 
- How is the existing Lexium 15 drive being controlled? Is it by analog signals or by fieldbus (CANOpen, Modbus...) 
Was this helpful?
What can we do to improve the information ?