Technical FAQs

Ask a Question

Are replacement CT's available for the 9065 Motor Logic Plus overloads?

 Issue:
Customer is trying to replace only the CT from the 9065 Motor Logic Plus overload

Product line:
9065 Motor Logic Plus II

Environment:
all

Cause:
Overload is not working

Resolution:
No replacement parts are available for the Motor Logic Plus.  The customer will need to replace the complete overload relay with a new product. 

 
Was this helpful?
What can we do to improve the information ?