Technical FAQs

Ask a Question

Is the 9999DD20 CSA approved?

 Issue:
Customer is asking if the 9999DD20 contact block is CSA certified.

Product line:
9999 DD20 8910

Environment:
all

Cause:
Product does not carry a CSA mark.  It does have a UL mark.

Resolution:
Yes, this accessory is CSA certified under cUL file NLDX8.E3190.  Howver the physical product does not have a CSAmark.

 
Was this helpful?
What can we do to improve the information ?