Technical FAQs

Ask a Question

Recommended ambient air temperature during normal operation of LXM32 drive

Issue:
Recommended ambient air temperature during normal operation of LXM32 drive

Product Line:
LXM32

Resolution:
Per the manual, the permissible ambient temperature during operation (no icing, non-condensing) is 0°...50°C (32..122°F). Within this environment there is no "derating" needed.
 
Was this helpful?
What can we do to improve the information ?