Technical FAQs

Ask a Question

When remote mounting keypad for the Process Drives, can the keypad be plugged into the lower Modbus port?

Issue:
When remote mounting keypad for the Process Drives, can the keypad be plugged into the lower Modbus port?

Product Line:
Altivar Process Drives

Environment:
All

Cause:
Would like to use the port behind the conduit cover, possibly for cable management purposes

Resolution:
Yes, the keypad can be plugged into the additional Modbus port and have the same functionality. 

 
Was this helpful?
What can we do to improve the information ?