Technical FAQs

Ask a Question

Looking to replace an ILA1B572S1839

Issue:
Looking to replace an ILA1B572S1839

Product Line:
ILA motor

Resolution:
The ILA1B572S1839 is a customized solution. It has a profibus interface that means movement commands and parameters are sent via profibus from a PLC. The machine builder or OEM has to be contacted to get it replaced or supported.
Was this helpful?
What can we do to improve the information ?