Technical FAQs

Ask a Question

Do Process Drives rated for 230v have an internal EMC Filter?

Issue:
Do the 230v Process Drives have an internal EMC Filter

Product Line:
ATV
 
Environment:
All

 
Cause:
Wiring

 
Resolution:
Per Level 3 in France;  The 230V Process Drives also have a filter board embedded, but the filter values are low to none.  So in 230V, it can be  considered that the product ATV..M3 have no EMC, because we are not compliant to EMC regulation. Some very low capacitor are present for EMC immunity.  However, it is possible to open the switch which remove the EMC connection of these little capacitors, if needed.
Was this helpful?
What can we do to improve the information ?