Technical FAQs

Ask a Question

Can the RMCN22BD have two analog input signals?

 Issue:
Customer wants to use two analog signals.  Will they need one of the RMCN22BD relays?

Product line:
RMCN analog Zelio relay

Environment:
n/a

Cause:
Documentation is not clear

Resolution:
The RMCN22BD can only have one analog input and one analog output. 

 
Was this helpful?
What can we do to improve the information ?