Technical FAQs

Ask a Question

What is the short circuit rating for VLS3P025D1 at 208V?

 Issue:
What is the short circuit rating for VLS3P025D1 at 208V?

Product line:
VLS disconnect

Environment:
all

Cause:
Catalog shows 5kA SCCR @ 575V. 

Resolution:
The 5kA rating does not change at lower voltages.  The unit is rated up to 5kA up to 575V applications. 

 
Was this helpful?
What can we do to improve the information ?