Technical FAQs

Ask a Question

What is Form Y56 for enclosed starters?

 Issue:
Customer is trying to match an existing enclosed starter and build up in the Product Selector tool.  Class 8606 with form Y56 that he cannot identify.

Product line:
NEMA starters, 8536 8538 8539, 8606, etc

Environment:
all NEMA enclosed starters

Cause:
Forms are not listed in any documentation.

Resolution:
Form Y56 on the old Enclosed NEMA starters was to provide a Brushed Stainless Steel, watertight enclosure. 
Form Y56 was replaced with Form G17 which is the same modification.  Both forms are obsolete and no longer available. 

Create a TAG request with the plant to request this type of modification.
Was this helpful?
What can we do to improve the information ?