Technical FAQs

Ask a Question

Do we send the Enclosed 8903L Lighting Contactors With Ground Bars on the Enclosure?

Issue:
Information if the Class 8903 Types L and LX Contactors comes with ground bars as standard

Product Line:
Lighting Contactors

Environment:
Class 8903 Types L & LX

Resolution:
Yes, ground bars comes standard on the enclosed 8903L & 8903 LX lighting contractors.
Was this helpful?
What can we do to improve the information ?