Technical FAQs

Ask a Question

Will removing the sticker on top of an ATV312 increase ventilation?

Issue:
Will removing the sticker on top of an ATV312 increase ventilation? 

Product Line:
Altivar 312

Environment:
All

Cause:
More drive ventilation needed

Resolution:
Yes, removing the sticker on top of the drive will increase ventilation. This is typically done when multiple ATV312 drives are mounted close together.
This process is described in the ATV312 Installation Manual (attached).

Was this helpful?
What can we do to improve the information ?