Technical FAQs

Ask a Question

Do we offer an enclosure for a 100% rated, 1200A, P frame breaker?

Issue: 
Since standard P1200 enclosures will not accept 1200A, 100% breaker, what size enclosure is required for a Powerpact P Frame, 1200A, 100% rated breaker?

Product Line:
Molded Case Circuit Breaker

Environment:
Powerpact P unit mount

Resolution:
Minimum enclosure size would be 62.25 in. H x 23 in. W x 14.75 in D.
 
Was this helpful?
What can we do to improve the information ?