Technical FAQs

Ask a Question

Are the Red and Black Pushbuttons Replaceable on the GV2M Manual Starters?

Issue:
Broken / Missing OFF-STOP and START pushbuttons

Product Line:
Motor Starters and Protectors

Environment:
TeSys™ GV Manual Starters

Resolution:
The red and black push buttons are not replaceable. The GV2M* manual starter itself must be replaced.
Was this helpful?
What can we do to improve the information ?