Technical FAQs

Ask a Question

Getting E4303 on the LXM32

Issue:
Getting E4303 on the LXM32

Product Line:
LXM32

Resolution:
This means that the LXM32 drive cannot monitor the temperature of the motor. It's a warning that shows when using certain 3rd party motors.
Was this helpful?
What can we do to improve the information ?