Technical FAQs

Ask a Question

What is the packing kit for VB-7213-0-4-0?

Issue:
Packing Kit for the FF Series / Current 1/2" to 2" VB-7xxx/ Discontinued 1/2" to 1-1/4" VB-9xxx/ VB-111, VB-121, VB-314, VB-334,VB-354 series Valves?

Product Line: 
HVAC / Field Devices

Environment:
Valves

Cause:
Replacement / Installation / Maintenance

Resolution:
YBA-622-2
Was this helpful?
What can we do to improve the information ?