Technical FAQs

Ask a Question

What replaces the DZ5CA162D?

 Issue:
Customer is asking for a replacement or alternative for the DZ5CA162D.

Product line:
DZ5
Environment:
DZ5CA162D

Cause:
DZ5CA162D was discontinued in the USA only due to low or no sales.

Resolution:
To answer your immediate need, it will be possible for you to replace by reference DZ5CA162, that will be similar but in white and compliant to NFC 63-023.  This is not blue like the DZ5CA162D which is compliant to DIN 46228-4.


 
Was this helpful?
What can we do to improve the information ?