Technical FAQs

Ask a Question

Is Modbus Plus available for the Altivar Process Drives?

 Issue:
Customer replaced an ATV61 drive with the new Altivar 930 drive and they need to communicate via Modbus Plus as the old drive was.

Product line:
Altivar Process, ATV630, ATV930

Environment:
all

Cause:
Communications

Resolution:
Modbus Plus is not available on the Altivar Process Drives.  Use a Modbus or Ethernet bridge and the built in Modbus or Ethernet ports of the Process drives.

 
Was this helpful?
What can we do to improve the information ?