Technical FAQs

Ask a Question

Can a single LTMR provide full protection for multiple motors connected at the same time?

Issue:
Can a single LTMR provide full protection for multiple motors connected at the same time?

Product Line:
LTMR series Tesys T Motor Control Systems.

Environment:
All models, All serial numbers.

Cause:

Clarification of operation.

Resolution:
The LTMR can not provide individual motor overload protection when multiple motors are connected.  The LTMR will protect against the total load of all motors combined but will not be able to detect the current draw of each individual motor when multiple motors are connected in parallel.
 
Was this helpful?
What can we do to improve the information ?