Technical FAQs

Ask a Question

What appliances can be used on circuits with Dual Function (CAFI+GFI) circuit breakers?

Issue:
Concern about appliances working with dual function circuit breakers.

Product Line:
Advanced Function breakers

Environment:
Residential

Cause:
Compatibly concerns

Resolution: 
Dual Function circuit breakers are designed for use in all residential living spaces.  It is best to check local electrical code requirements and appliance manufacturer's
install guides ahead of installation.
Was this helpful?
What can we do to improve the information ?