Technical FAQs

Ask a Question

Does Square D offer a lug kit to allow a larger Main phase and Neutral wire for voltage drops in the 125amp QO and Homeline load centers?

Issue:
Product Design Features

Product Line:
QO and Homeline Load Centers

Environment:
Accessory


Cause:
Application

Resolution:
There is a lug kit available, part number QOL125VD.
This lug kit will ONLY allow for (1) #4 - 2/0 AWG Max. Cu wire or (1) #4 - 4/0 AWG Max. Al. wire and can ONLY be used in the Homeline, Series S04 or higher and the QO, Series S06 or higher, 125Amp MAX, single phase load centers marked appropriately on the Wiring diagram in the accessory table. 

EXCEPTION: Wire Bending Space does NOT permit use of Aluminum wires larger than 2/0 AWG in the following load centers = QO120L125GC, QO120L125G and QO12024L125G.

NOTE: DO NOT EXCEED THE MAXIMUM AMP RATING OF THE LOAD CENTER.

SEE BELOW ATTACHED INSTRUCTION SHEET
Was this helpful?
What can we do to improve the information ?