Technical FAQs

Ask a Question

What marking cards are compatible with NSYTRAPLOT?

 Issue:
Customer wants to know if competitor cards are compatible with the NSYTRAPLOT.

Product line:
Linergy NSY marking

Environment:
n/a

Cause:
n/a

Resolution:

The NSYTRAPLOT is compatible with the following cards.
 
  • ZBY type legend
  • HP plotter pen
  • TRA type marking card
It is not compatible compatible with other manufacturers labels.

 
Was this helpful?
What can we do to improve the information ?