Technical FAQs

Ask a Question

What are the dimensions of an MK-8801

Issue:
Dimensions of an MK-8801, MK-8811 and MK-8821 actuator.

Product Line: 
HVAC / Field Devices

Environment:
Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
(11-3/4in height) x (10-1/2in wide) x (10-1/2in deep)
(298mm height) x (267mm wide) x (267mm deep)
Was this helpful?
What can we do to improve the information ?