Technical FAQs

Ask a Question

Can the plastic gear in Classic Erie Zone valve repair kit 630-240-1 be supplied with a metal gear ?

Issue:
Classic Erie zone valve repair kit 630-240-1 used to have a Metal gear , now it's Plastic. Can a metal one be ordered?

Product Line:
Valves and Actuators

Environment:
Maintenance

Cause:
Repair kit 

Resolution:
The current repair kit 630-240-1 is now supplied with a Plastic gear and the Metal gear, previously shipped in the Kit, is not available in kit form or seperately anymore.

 
Was this helpful?
What can we do to improve the information ?