Technical FAQs

Ask a Question

What is the NEMA rating of an AL-150?

Issue:
NEMA rating for AL-150 and AL-151 Solenoid Air Valves?

Product Line: 
HVAC / Field Devices

Environment:
Application

Cause:
Product Features 

Resolution:
The Solenoid valves have a NEMA Types 1, 2, 3, 3S, 4, and 4X rating 
Was this helpful?
What can we do to improve the information ?