Technical FAQs

Ask a Question

What are differences of the following actuators MS51-7203, MS51-7203-40, MS51-7203-50?

Product Line: 
HVAC / Field Devices

Environment:
Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
The differences of these Actuators are the default control signal;
MS51-7203 has a (2-10vdc) control signal
MS51-7203-40 has a (6-9vdc) control signal
MS51-7203-50 has a (0-10vdc) control signal

 
Was this helpful?
What can we do to improve the information ?