Technical FAQs

Ask a Question

How do I determine the firmware or application version of my RealStream controller?

The firmware version running on the RealStream controller is not directly available, unless using ClearSCADA, or reading a Modbus register with the Version Number in it.

The local display gives a station version, which can be found by logging in:

Main Menu -> 1.1 Overviews -> System Overview -> App Ver. or FW Ver. (scroll to the bottom)
Was this helpful?
What can we do to improve the information ?