Technical FAQs

Ask a Question

Can I set the deviation in RealStream on a point that generates an event in DNP3?

No, these deviations are set as part of the factory programming to maximize the amount of useful data, while minimizing the overall event count.
Was this helpful?
What can we do to improve the information ?