Technical FAQs

Ask a Question

What are the main bus ratings for the CHOM1632M**GC load centers?

Issue:
What is the main bus rating for Homeline Load Centers CHOM1632M30GC to CHOM1632M100GC?

Product Line:
Load Centers

Environment:
Homeline

Resolution:
 Per the attached wiring diagram, the main bus ratings are maximum 100 amps.
Was this helpful?
What can we do to improve the information ?